Part Number: PGA450Q1EVM
Other Parts Discussed in Thread: TIDA-00151, PGA450-Q1, PGA460-Q1
I am developing a pcb with a pga450q1. I wanted to communicate my microcontroller through uart port. I have right now a pga450q1evm and a TI-151.
Thanks to the ti ger board, I have seen the data comming throuh FIFO and it works fine. I could modify all ESFR registers to work with my transducer and measures are quite good.
Now I am trying with the smaller board (ti-151) and uart. I have tried so far to use command 0 to see if it is working, command 1 to fire a burst and command 5 to read all FIFO values.
I can generate a chart with the values from FIFO but they are not very accurate. I think I'd need to update ESFR parameters to work with my transducer too as I did with TI GER board.
I have seen there is a command (comm 3) to update EEPROM values but I haven't seen one for ESFR. Is there a way to do this? Could I update ESFR parameters through uart?
In case it is possible, could you show me an example? Or point me to a document where it is explained.