Part Number: DAC3174
DEARS.
Customers use the AD9746.
The reason for using the AD9746 is as follows.
The AD9746 provides the following features.(AD9746 Datasheet 27page)
[The user can place a carrier anywhere in the first three Nyquist zones depending on the operating mode selected.
The performance and maximum amplitude in all three zones are impacted by this sinc roll off depending on the placement of the carrier.]
Does DAC3174 provide three Nyquist zone?
Are the functions of the AD9746 included in TI's products?
What is the TI Competitor part for the AD9746?
Thank you.