Part Number: TSW40RF80EVM
Other Parts Discussed in Thread: DAC38RF80
Hi,
I recently purchased and received TSW40RF80EVM (together with TSW14J56).
A couple of issues:
- There is no BOM, schematics or gerber files online. Could you provide these for a design reference?
- I would like to use the DAC38RF80 without the internal synthesizer, feeding directly with a high speed clock ( >6GHz)
How can i be sure that i'm meeting the sysref to devclk setup and hold time? the data sheet mentions a sysref capture circuit,
can i use this option with the TSW40RF80EVM?
Is there a test point i can use to probe sysref and device clock with a scope? ( the IC has a heat sink on top it, so there is no space to place a probe)
Best Regards,
Guy.