Part Number: ADC32RF45
Reviewing the data sheet, there are some questions regarding the spurs shown in the FFT responses. In particular, when looking at Figure 4 which shows the FFT for a 900 MHz input tone.
Data sheet specs indicated SFDR at 900 MHz input is 77 dBc, excluding HD2,HD3,HD4, HD5, and interleaving spurs IL and HD2 IL. In Figure 4 we can identify these spurs, but would like to know more about the non-HD2/HD3 spurs identified as -84 dBc and the IL spurs at -79 dBc in the figure caption:
1. Are these spurs dependent on input signal amplitude? Will they go down in amplitude with the input, and at what rate?
2. We can identify the IL and harmonic spurs in the FFT plot. What are the sources of the other spurs? are they clock related? Would they scale down under certain conditions?