Part Number: ADS1191
Hi,
I am using ADS1191 to sample ECG signal. I have finished the driver and get the signal data. I test the following signal:
1) set CH1SET=0x01, get the signal with Input shorted, then the output value is about +-5, this is right.
2) set CH1SET=0x05, CONFIG2=0xE3, get the signal with internal test signal 1Hz, and the positive peak is about 80, negative peak is -80, and the waveform is right also. 1Hz 1mV test waveform.
3) set CH1SET=0x00, CONFIG2=0xE0, get the signal from my left hand and right hand, but this step get stuck, I could not get any ECG signal from the output, all data is noise, after filter, nothing.
Could you help to advise what way can I try? Is there any point missed by me?
Regards
Simon