Part Number: DAC38RF83
Dears.
Customer is developing DAS.
The frequency range is from 700 Mhz to 2600 Mhz.
When Balun(1:1) is applied to the DAC38RF83 output, a large loss difference occurs depending on the frequency.
EVM uses Balun(2:1). Is there a reason for that?
Have to use only Balun(2:1)?
In the data sheet, it is 100 ohms.
The actual pattern of DAC38RF8xEVM is thick.
Impedance matching value of Balun of DAC38RF8xEVM?
Thank you.