This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DAC5573: DAC5573 with single power supply

Part Number: DAC5573


HI,

I am using DAC5573 with single power supply of 5V.
The DAC5573 should have the range from 0 to 255, but it seems to have the range from 0 to 127 only.
When I set the value 80h-FFh the output voltage is same as when I set to 7F.

Is this correct operation ?