This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

About recommended products

Other Parts Discussed in Thread: DAC2932, DAC2900

Hi,

Customers are looking for products that meet the following specifications.
(looking for products as close as possible)

・Resolution Bit:over 8bit
・Sample/Update Rate:about 125MSPS
・Power Consumption:Low power as possible

Product image is below.
http://www.analog.com/en/products/digital-to-analog-converters/ad9714.html
Could you tell me your recommended products?

Best Regards,
Yusuke/Japan Disty

Power Consumption

  • Yusuke-san,

    I would recommend looking at DAC2900 operating at 3.3V; this part meets the sample rate and resolution requirements. If the customer is flexible on sample rate then I recommend using the DAC2932 which is very low power consumption and offers 12-bit resolution with a maximum sample rate of 40MSPS.

    Best,
    Mark