Dear Team,
My customer is having 2 ADS8568 chips on board on top and bottom on a few cm distance from their FPGA.
They are reporting that once every few power ups the ADC is waking up in a state where it's internal Vref is very close to zero resulting wrong readouts.
They are using the internal Vref.
The phenomena is very hard to duplicate but is still occurring from time to time.
The two ADCs are configured to the exact same configuration using the same commands.
Even if the customer does not configure the ADC and work in the default mode - this phenomena still occurs.
In addition the phenomena always occurring in the same (bottom) ADC. They have assembled 4 boards and the phenomena is consistent across all the four boards.
Do you know of any such issue with the ADS8568 ?
Can you help us debugging this ?
Can this be occurred maybe due to slow/fast slew rates of the VCC ?
Best regards,
Nir