Part Number: DAC7728
Hello,
I have design a pcb board, which 2 DAC7728, my configuration:unipolar output, i don't use the correction engine, 15V for AVDD, IOVDD is connected to DVDD and is 5V, i dont use LDAC
Some time one is not starting (all time the same), and any command i will send is not executed. (ex: test GPIO)
I restart the board, and this is ok.
I give my schematic:
The power supply +24Vana is configured to 15V.
The DVDD is set firt, and AVDD and REFA/B.
I have had pull up (47K) in CS pin of DAC, no change.
Do you have timing specification for the setting time of power-supply?
Or is it other problem?