Other Parts Discussed in Thread: ADS1158, REF3125
Hello,
I am currently working on a DAQ board project using the ADS1158. So far, every doubt I had was answered either by the datasheet or by several of the application notes concerning TI ADCs. However, there is one thing with which I am stuck, and that is the use of separate analog and digital ground planes. No matter how hard I look for answers, this seems to be something that depends on a personal taste, and being an inexperienced engineer doesn't help much.
Straight down to my question... specifically for the ADS1158, should I use separate analog and digital ground planes, or does a single ground plane suffice, provided that
I use adequate filtering for my analog supplies? What would be the best way to lay out a board for the ADS1158?
The power supply on the board consists of an LM2673S switching regulator (Fosc = 260kHz) which provides 7V to a REG104-3.3, a TLV70025, and to an LM2575S configured as an inverter (Fosc = 52kHz) which provides -3V to a TPS72325 regulator. The output of the LM2575S is filtered by an LC filter (22uH, 100uF). The ripple at the output of both switching regulators (on a custom-built eval board) doesn't exceed 10mVpp (measured with a Fluke 105B scope).
The +2.5V/-2.5V from the TLV70025 and the TPS72325 provide the analog supply to the ADS1158 and the REF5040 laid out exactly like the example in the datasheet. The output of the REG104-3.3 powers the rest of the board (LPC2478 microcontroller, DP83848IVV Ethernet PHY, MAX3243UI drvr/rcvr, MCP2551 CAN transceiver).
USB Vbus lines, as well as the grounded shields, are filtered with ferrite beads (Murata BLM21PG221SN1D, 220 ohm @ 100 MHz).
Thank you very much.
Best regards,
Pablo