Other Parts Discussed in Thread: DAC38RF82, TIDA-01435
Hello everyone,
I am trying to use the DAC38RF82EVM to generate wideband IQ baseband signal. I am using the settings for the Dual DAC mode as described in the User guide available on the product web-page. the output signal of the DAC is captured using an oscilloscope and the constellation (QPSK) is plotted using Matlab. The constellation is extremely scattered with a best EVM (error vector magnitude) of 9%. I have tried to reduce the symbol rate (from 500 MHz to 50 MHz) but the performance becomes even worse (14% EVM for 50 MHz case).
However, the results are far better if a bandpass signal is generated using only the DAC A and the digital mixer of the DAC-EVM. In this case, I use the same oscilloscope and digitally down-convert the signal in Matlab to plot the constellation (with an EVM of less than 2%). In this case, symbol rates as high as 625M could be demodulated with good performance.
I wonder if the DAC-EVM is even intended to be used as baseband signal generator or there is some settings in the GUI or signal path which I am not correctly using.
Best Regards,
Saad