This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADC128D818: Input current during sampling and input capacitance

Part Number: ADC128D818

Hi support team.

My customer is considering to use the ADC128D818 for temp monitoring system.

They want to know the value of Input current and input capacitance during sampling .

Could you please provide the data or information?

Best regards.

Higa

  • Hi Higa,

    Let me see what I can find out about the sample capacitor on the ADC128D818 and I'll get back to you as soon as I can.
  • Hi Higa,

    The S/H capacitor would be on the order of 10-12pF. Regarding the input current - this value is not normally specified beyond the ABS MAX value of current into any one pin, which is +/-5mA (see section 7.1). When you say the application is temperature monitoring, are you using only the internal temp sensor or are you planning to add RTD's and/or thermocouples to the analog inputs?