This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Dear all
I have a confusion about some parameters of DAC8218's digital IOs.
1. As for the GPIOn, in absolute ratings, it shows maximum current is 5mA. I want to know whether this is maximum output current or input current, or the logic driving current?
2. As for the USB/BTC, RSTSEL, etc. logic input pins, here the input current is only ±5uA, I want to know the meaning of this value. Should it be the input leakage current? Or should it be the maximum driving current, which means the master should provide 5uA driving current at least?
3. The datasheet mentioned that the digital IO pins should be pulled up to VDD, I want to know how to calculate the value of pull-up resistors.
Thanks.