Other Parts Discussed in Thread: ADS1298ECGFE-PDK, ADS1298
Hello,
I recently connected teh ADS1298ECGFE-PDK demo unit and trying to configure it to measure 0-4V. I belive I have the ADS1298ECGFE Eval software configured correctly but when ever I take a reading, my mreasurement max out at 2.5 V. I tooked at the TP3 (VREFP) and noticed that it was ~+1.5V (relative to AGnd) when the spec stated its should be +2.5V. I measured VREFP reltative to VREFM (cathode side of C1 pad) and noticed that was the expected +4V. Could I have misconfiguered something that might cause the VREFP at a voltage other than 2.5V.
Thank,
Ben