This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DAC3484: DAC3484

Part Number: DAC3484

Hi Timothy,

Thanks for the reply and explanation!

The current LMK04828 settings:

DCLKout2 register 0x108 = 0x01; The divider value is 1; The DCLKout2 frequency is 2,457.6 MHz.

DCLKout12 register 0x130 = 0x05; The divider value is 5; The DCLKout12 frequency is 491.52 MHz.

This DCLKout12 clock is the DAC3484 DACCLK input.

In DAC3484 DATACLK input is 122.88 MHz.

I need to change the DAC3484 DATACLK  from 122.88 MHz to 153.6 MHz.

Does it mean if I change the DAC DATACLK to 153.6 MHz from 122.88 MHz I will also have to change DAC3484 DACCLK to 614.4 MHz from 491.52 MHz by changing the divider in LMK register 0x130 to 0x04 from 0x05? 

I am not sure how to re-post the same question to the DAC group.

Could you please help me with this as well?

Thanks,

Mike