This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ads1262: Is there a reference design which showes the interface between ads1262 and TI's am335x CPU

Part Number: ADS1262
Other Parts Discussed in Thread: ADS1262, TIPD188

Hi, there

I am not sure this topic should be posted here or Sitara forum.  Any advice about this? I think SPI interface should be used. But what should do to drdy pin?

Thanks

Yang

  • Hi Yang,

    We don't have any ADS1262 example code that is specific to a Sitara CPU, but there is an example project for the ADS1262 (and MSP430) found here:

    (or go to the TIPD188 page and look for the Firmware file under the "Software" heading).

    Hopefully, that example code can help with the higher-level communication between the MCU and ADC once you've got the SPI working. I'd expect there to be some other example code, more specific to the Sitara which would show you how to get the lower-level SPI working.

    I'm more familiar with the ADC side of things, so please let me know if I can help you out with any other questions you might have related to the ADS1262!

    Best regards,
    Chris

  • Hi, Chris

    Thanks for your help sincerely . I think I should post this thread on Sitara forum.

    BR
    Yang