This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DAC8750: How long does it take to complete the reset after writing 0x01 to the reset register?

Part Number: DAC8750

Hello.

The datasheet says:

8.6.1.4 Reset Register
The DACx750 reset register is written to at address 0x56. Table 17 provides the description.

Table 17. Reset Register
DATA BIT(S): DB0
NAME: RESET
DEFAULT: 0
DESCRIPTION: Software reset bit. Writing 1 to the bit performs a software reset that resets all registers and the ALARM status to the respective power-on reset default value. After reset completes, the RESET bit clears itself.


Question:
How long does it take to complete the reset after writing 0x01 to the reset register?


Best Regards.

  • Sato-san,

    I have responded in your other thread. As this appears to be a duplicate, I will recommend this post as the answer and please request that you confirm this as an answer so we can close this thread.

    We will continue the discussion in the other thread.