This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ads8319: Missing codes at higher Signal levels

Part Number: ADS8319
Other Parts Discussed in Thread: ADS8319

Hi,

I have the following Problem with ADS8319:

Resolution seems to degrade with Input Signal Level.

I am using ADS8319 at 3.3V digital and 5V analog supply and reference. I am using 3 wire CS mode with busy indicator.

At Input signals close to 0V LSB (D0) is giving correct values (i.e. it is changeing)

At Signal Levels of about 4.5V D0-D2 are always 1 (also verified through measurement with oscilloscope on SDO) - so efective Resolution is 13 bits instead of 16.

The higher the signal Level gets, the more missing codes respectively less effective Resolution I am getting.

Any idea ?