Other Parts Discussed in Thread: ADS1256
Hello,
i want to use the ADS1256EVM board, but somehow fail to get the thing "running". ( DOUT stays low, doest matter what i do ... )
To test my setup and to reduce possible mistakes on my part, i only supply the board with 5V on +5VA, 3.3V on +3.3VD and the
ground on DGND. Jumpers are all set to default.
On D0 i can see the 7.68Mhz crystal working, so i guess the ads1256evm should be working ? (Tried a second board, same thing ... )
With this set up I assumed to see an periodic state change on DRDY but, DRDY stays high. (should this be?)
Did i miss something? Do i have to enable the ADS somehow?
thx