Other Parts Discussed in Thread: ADS4145
I am planning to use the ADS4145 in low speed operation (<20Msps). I had a concern regarding this. The datasheet recommends using this part with CMOS interface at low sampling speeds for lower power and better setup/ hold times.
For our application, this ADC will interface with an FPGA tied to 2.5V bank voltage, and i cannot change this bank voltage. The 1.8V CMOS interface from the ADS4145 will marginally make the Vih requirements. So i wanted to check if there are performance issues in using this part in LVDS mode for low sampling speeds ? Will the part provide good SNR, SFDR or is there significant degradation ?
Thanks,
AB