Part Number: DAC38RF83
I am trying to write a set of isolated SLI write functions to modify specific parameters within the DAC and not impact the remainder of the device.
1. specify the multi-duc and the path, then change the mixer gain from 0 to 6 dB.
2. specify the multi-duc and the path, then change the voltage gain, i.e, GAINAB or GAINCD.
3. specify the multi-duc and change the coarse gain, i.e., DACFS.
4. specify the multi-duc, the path and the nco and change the nco frequency, i.e., FREQ_NCOAB or FREQ_NCOCD.
I believe that what I am looking for is related to auto-sync, though my experimentation has not been yielding good results.
At this point I am looking into errors related to FPGA register mapping and the interface with the SLI read/write function in the FPGA. Once this is debugged, I would like to be certain that the targetted register writes are correct for each of these functions.
Can someone provide the register writes required for these functions?
Thanks,
Phil