Part Number: TSW14J56EVM
I loaded the HSDCpro application and installed the additional FPGA firmware (and placed it into the HSDCpro's directory). My computer is not able to identify any drivers when I plug it in via USB (it recognizes the USB itself, but nothing else). I tried giving all the resets possible with SW11 (and the main reset switch for the power), even unplugging the system and plugging and repowering it into different ports, but the errors still seem to be prevalent. I uninstalled the program and reinstalled version 4.70 into my computer, even adding in the firmware a second time, but it still does not seem to identify any buses or drivers correctly. Are there any methods to help properly identify these drivers and buses so I can load the firmware and HSDCpro can properly identify the TSW14J56 EVM?