ADS1298 system with Right Leg Driver multiple chips, 1 chip generates reference 3.0v system, High Resolution, 10K samples per second useable...
What I am trying to do now is set the registers for the ads1298 by using a xilinx FPGA. I want to set the clk in the fpga to the clk to the ads1298 for 10ksps or maby higher in the fpga and divide it down for the ads1298.
Then the SCLK should be clk/4=sclk so loading the registers their is not a delay.
I know I am interested in a system with 10K SPS their will be multiple chips with a shared voltage reference created by one of the chips. They should all be set to High Resolution the systems should run at 3v. The Right leg driver multiple chip option would be used as shown how multiple chips can have 1 DRL then before that how the DRL circuit is configured.
So how would you sugjest how the registers should be set? The ones with the defalts allready ok.
What pages on the data sheet should I refer to?