Part Number: ADS1120-Q1
Hello,
Regarding to Bridge Measurement with ADS1120-Q1, my customer is asking a question.
They will refer Figure 82( Bridge Measurement ) on datasheet(page 95) for their application.
・Analog input : Magnetic(Hall) Sensor
・AVDD = Magnetic Sensor power: 5V
・Data rate: 2k SPS
(Question)
(1)They will place a current limit resistor between power line and power input,
because magnetic Sensor can’t input many current to power input.(Please refer below.)
In this case, is there any problem or concern?
(For example, the impact on ratiometric operation)
(2) A first-order differential and common-mode RC filter(RF1, RF2, CDIF1, CCM1, and CCM2)
How much resistance value and capacitance value should they estimate?
Can they refer Thermocouple Measurement section on datasheet(page48)?
(RF1 = RF2 = 1 kΩ, CDIF = 100 nF, and CCM1 = CCM2 = 10 nF.)
Regards,
Tao2199