Part Number: ADS8405
1. Is there any requirements for the power sequencing of ADS8405 since there are two power supplies (VA and VDB) ? I can't find any information about that in the datasheet.
2. Can I place capacitors on REFOUT pin even if I use an external Vref connected to REFIN or should I remove them (dual-version board with options)?