This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TSW14J56EVM: Question about file size

Part Number: TSW14J56EVM


Hi I am using the TSW14J56EVM board and was wondering what is the limit on the file size which can be sent to the board?

  • Hi Dillon,

    The TSW14J56 has 4x8Gb DDR3 memories.  This translates to 32Gbits of storage.  or 2Gsamples of 16 bits.

    I believe the memory is split into TX and RX memory so you should be able to load in a file that contains 1Gsamples of data.  Although this is possible, it may not be practical due to PC system limitations and transfer speed from the PC to the TSW14J56 EVM.

    Most of the large files that we have used have typically been 10ms frames of data - this could be upwards of 10-20Msamples.

    Ken