Part Number: ADS52J90EVM
Other Parts Discussed in Thread: ADS52J90
Dear all,
I am having a few difficulties in setting up the two EVMs in order to detect a sample frequency given via function generator. In HSDCpro, I have downloaded the appropriate firmware and have selected the ADS EVM as my main ADC for capture. For inputs, I am using a 5 MHz square wave for a clock (J75) and a 100 kHz sinusoidal wave as my test function in pin (SMA_CH4). When I try to capture this data, I get a message seen pictured here:
I took a look at the TSW board and currently the D4 LED is unlit and the D3 is still ON. I made sure everything was reconnected and not reset (as seen in the first suggestion) and am looking for a bit of help in order to give a custom sample (I am very new to FPGA programming and configuration so I need all the assistance I can get).
Is there anyone who can help? It would be much appreciated since I have a very limited amount of time to get test samples running.
Thanks,
Christopher Harness
Also, is it known as to whether or not the TSW EVM series contain internal clocks, thus eliminating the use of external ones? If so, how is that configured or utilized?