Part Number: DAC38RF82
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: DAC38RF82
Jenny,
Can you use real input data, not IQ? With real input data, you can use only 1x or 2x interpolation factor. At 1X, the line rate will be 5.625Gbps. At 2x, half this rate. This will require a LMF = 413. If you require IQ input data, you will have to use 2 IQ pair inputs and 24x interpolation. The LMF = 243 for this case and the line rate will be 1.875Gbps. These are the only options available unless you change to some other setting.
Regards,
Jim
Hi Jim,
Jenny,
I cannot get this to work with your numbers in 12 bit mode. If you use dual DAC 14 bit mode, you can use 1 I/Q pair, 6x inter, and get a serdes rate of 5.625Gbps with the input data rate at 562.5MHz and the DACCLK at 3375MHz. Will this work for you?
Regards,
Jim