Part Number: DAC7551-Q1
Hi,
When a resistor is connected to the VREFL terminal of the DAC7551-Q1, you want to check the effect of the VREFL(3) pin.
Since we want to output approximately 0.7V to Vout when Code= "0"
When a resistor is inserted and connected between the VREFL(3) pin and GND(6),
Is there a possibility of damaging the device?
For example, the VREFL terminal is damaged when the power is turned on or during normal operation?
※ Since the internal resistance accuracy is ±20%,
I understand that it is not recommended to connect a resistor between the VREFL terminal and GND.
Best Regards
cafain