Part Number: ADS1220
Other Parts Discussed in Thread: ADS124S08
I am comparing ADS1220 and ADS124s08. Obviously the latter has a more extensive feature set, but notwithstanding, I want to understand the power usage of these two devices.
In my application, I plan to take an ADC reading (and maybe a temperature reading from an external diode, which requires changing the PGA setting....), then falling asleep for x seconds (from 1 to ??? seconds).
Can anyone on this forum give a rough estimate of how much current is consumed during the waking portion, and sleeping portion of this cycle, so I can make some meaningful calculation on battery life? Of course I will need to add the microprocessor in the mix (MSP430, or Bluetooth micro in a module), but I'm just talking about the AtoD in this case.
I plan to power a 5k bridge with the internal reference, current mode (at the lowest uA that I can get a good reading), PGA at 16 to 64 (depending on bridge sensitivity).
The ADS1220 does not give very much information about current consumption (unlike the ADS124s08 datasheet). It advertises 120uA in duty cycle mode (is this average current through a duty cycle??), where the duty cycle sample rate is 5SPS minimum. I don't need 5SPS in my particular application. So I will be probably manually putting the 1220 asleep, in the same fashion as the 124s08. The 124s08 advertises "Low Power Consumption: As Low as 280 µA", but I can't find in the data sheet which mode this is in or the conditions surrounding it.
I am really looking for two answers, with the first being somewhat vague:
1) relative current, as in "the 124S08 will consume half the power of the ADS1220" in the mode described above.
2) a ballpark estimate of consumption (for each ADC) during sleep and wake functions, as well as how long it will be in each mode (i.e. it takes x ms to wake up, take a reading from a differential pin pair, switch the PGA to a different value, take readings from a second pair of pins, switch back to the original pin pair (prep for next cycle), then fall asleep for x ms) within a one second cycle.
Thanks in advance!!