Other Parts Discussed in Thread: TVP5158
Hi
It is quoted in SLEA073A TVP5158 Layout guidelines as follows:
· VIN_x_P and VIN_x_N should be routed side by side as differential lines. The clearance between two
traces should two to three times the trace width.
· Maintain a CVBS video input trace impedance of 75ohm.
My concern is that, according to our stack up, to route VIN_x_P and VIN_x_N lines as differential, with 75 ohm impedance, we have to route it with 6 mil trace width and 4 mil tolerance, which violates the 1st point quoted.
Please let me know if it is ok to proceed?
Regards
Sushruta