Part Number: ADS131A04
Other Parts Discussed in Thread: ADS131A02
The key question is - are there any limitations in bandwidth if we are daisy chaining 3 ADS131 chips together and running it at max 128ksps (in Synchronous Master Interface Mode, or any other modes)? If so, what are the recommended solutions around this.
We're planning to daisy chain 2 ADS131A04 and 1 ADS131A02 together to string together a total of 10 channels. Looking at the SPI bus timing requirements and the amount of data being sampled, we are concerned with the bandwidth limitations.
Based on our calculations -
Min SCLK Period = 2x 56ns = 102ns (Synchronous Master Interface Mode)
Max SCLK = 15.625 MHz
Max Data Rate = 1.95MB/s
Max Frequency 128KHz
Required Bandwidth = ((16 bit depth x 4 channels)+16 Overhead bits)*2 chips+((16 bit depth *x 2 channels) + 16 Overhead bits) * 128KHz = 3.25MB/s
Required Bandwidth > Max Data Rate
Based on our calculations, there is a bandwidth limitation. We also think the time between nDRDY to the next nDRDY does not provide sufficient time to transmit data from the 3 ADS131 chips.