Part Number: ADS1292
Other Parts Discussed in Thread: ADS1294, ADS1298, THS4551, THS4521, TINA-TI
Hello,
I'm using the ADS1292 for EMG signal acquisition. My circuit has filtering and amplification stages before feeding the signal into the ADS1292, so the input signal will be single-ended. According to the data sheet differential input is recommended and I understand the advantages of doing that, but as it is not suitable in my application I need to go the other way. Means I drive the negative input INN to mid-supply using a voltage divider. I'm just wondering if my design is correct. I need to admit that I'm new to this field and I couldn't find appropriate answers to my problem in this forum.
1) is the circuit for the single-ended input correct like I do? Are there better ways to provide the mid-supply than using a voltage divider?
2) does it work together with the single voltage supply I provide? (AVDD = 3.3V , AVSS = 0V)
3) according to the data sheet, the RLDIN/RLDREF can also be used as single ended input. Is that a better way to go? But I still like to use the Right Leg Drive...
Thank you for your support