Hello,
Do we have suggest 12-16 channel ADC to meet below customer voltages? Resolution is not critical. Thank you.
0.6V, 1.2V. 0.8V, 12V, 3.3V, 1.5V
BR
Patrick
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Patrick
Please take look at ADS7952 / ADS7953 devices. These are 12/16 channel, 12 bit, 1MSPS ADC. It addresses most of the input voltage range you are asking for except 12V. for anything above 5V input range you can use resistor divider scaling at the input of ADS7953
Thanks & Regards
Abhijeet