Hi everyone,
I need a little help selecting an ADC for the output of a Wheatstone bridge as I am far from an expert on ADCs. The sensor I am using is not perfectly tuned so the bridge reads about -100mV to 2.4VDC instead of a perfect 0 to 2.5VDC. What is tripping me up is the fact that I have a negative differential voltage, does that mean I need a bipolar ADC? This is for an industrial level sensor that is only polled once a minute so the ADC does not need a fast sample rate. We are using a low cost AVR microprocessor so I2C or SPI is needed for interfacing.
Thanks