Part Number: PGA900
One, because there are films contained M0 chip, but I see the program storage is OTP, so inconvenient follow-up procedures to upgrade, I do not know there is no solution?
Second, if you do not use M0 microcontroller function (that is, in Reset mode), can achieve two-way data acquisition, temperature compensation (compensation level)?
Third, if you do not use M0 microcontroller function (that is, in Reset mode), can achieve the acquisition of data through I2C or SPI upload to the main chip? OWI for the receiver has additional decoding circuit requirements, not very convenient.