Part Number: DAC34SH84EVM
Hej all,
I am using DAC34SH84EVM rev D (which I guess it is reference D) and FMC-DAC adapter rev D. I did cut off the tab to make them being able to connect.
Now I have another issue that make me confused
1. At DAC34H8x EVM Interface (rev D) pins at 180-pin connector are different with the pins at FMC-DAC adapter rev D, while at DAC34H8xEVM rev C the pins at ASP-122952-01 are compatible with FMC-DAC adater rev D. It means that I have to change the board to rev C, doesn't it?
2. In the FMC-DAC adapter, there are 4 pins (they are IO-DB1P-N, IO-DB0P-N) not being available on the FMC connector. They are available on the connector ASP-122952-01. Is this a bug?
Thank you for your help.
Long