Other Parts Discussed in Thread: ADS1118, ADS1115, ADS1100, ADS1203
I am new to TI parts. My project involves monitoring an input voltage and setting up an output based on the input voltage. My supply voltage is between 3.2V and 4.2V (battery power), the input to sample is .5V to 3 V. I would like a small package, 6 to 8 pins. When I use the various part selection tools TI has I come up with large chips, maybe 32 pins.
I'm sure it is just my inexperience using the tools that is the main problem. I have tried several times but can't seem to find what I want. I have done this project with a microchip but really want to move to TI.
Can someone recommend some ADC parts for this?
thanks in advance