Other Parts Discussed in Thread: ADS1258
I have a couple of questions about this converter:
1) If I read the datasheet correctly one could start the converter in autoscan mode with all 16 channels selected and never stop it.
And then read the channel data as needed with Channel Data Read Commands. Is this correct?
2) Very little is said about the Channel Data Read Command.
For Register Read Command automatic incrementing of register address is discussed.
But there is no mention of a similar index for Channel Data Read Command. I assume that the device behaves this way.
Is this correct? If so, does Channel Data Read Direct also work with a auto-increment mechanism?
3) I seem to be having a problem with the Register Write Command. I follow each of these commands with a Register Read Command but
I do not always get the value that I just wrote. The device behavior also seems to indicate that the write did not occur properly.
4) In Autoscan mode it appears that DRDY asserts at the end of each conversion cycle - if one channel is selected after it is converted
(approx. 43.75 us) - if 16 channels are selected after it has converted all sixteen channels (approx. 700 us, 1.4 ms if CHOP is enabled).
Is this correct?
Charlie