This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DAC38J82: DAC38J82 - IMD3 SPECFICATIONS NOT MET DC TO 500 MHz

Part Number: DAC38J82

Hi,

 We tested our DAC - DAC38j82  for the frequency range of 20 - 500 MHz, two tones are provided with 1MHz spacing. We have not achieved the specified results as per datasheet.

Test Condition : Fdac - 1200 MSPS , Interpolation - 2x and PLL - ON IoutFS -20 mA , @-6dBFs.

Direct DAC Output
S.No F1 (MHz) F2 (MHz) 2F1-F2(MHz) 2F2-F1(MHZ) P1 (dBm) P2 (dBm) TOI P1 (dBc) TOI P2 (dBc)
1 21 22 20 23 -8.34 -8.35 -86.19 -96.65
2 30 31 29 32 -8.32 -8.32 -83.97 -93.84
3 40 41 39 42 -8.24 -8.24 -82.21 -93.9
4 50 51 49 52 -8.2 -8.21 -80.37 -88.58
5 60 61 59 62 -8.23 -8.23 -79.57 -88.53
6 70 71 69 72 -8.19 -8.18 -76.8 -87.7
7 80 81 79 82 -8.13 -8.13 -75.23 -82.35
8 90 91 89 92 -8.11 -8.12 -74.1 -81.4
9 98 99 97 100 -8.12 -8.13 -73.6 -81.8
10 101 102 100 103 -8.13 -8.13 -73.2 -80.7
11 150 151 149 152 -8.21 -8.21 -69.8 -75.2
12 200 201 199 202 -8.31 -8.32 -66.15 -74.18
13 250 251 249 252 -8.49 -8.49 -62.38 -77.16
14 300 301 299 302 -8.654 -8.63 -59.9 -91.03
15 350 351 349 352 -8.88 -8.89 -58.14 -84.17
16 400 401 399 402 -9.09 -9.102 -57.71 -70.86
17 450 451 449 452 -9.052 -9.051 -55.38 -70.95
18 498 499 497 500 -9.342 -9.36 -54.18 -67.19

Is there anything to be look for in DAC settings?

Regards

Balaji.