Part Number: TMS320C28346
Other Parts Discussed in Thread: ADS7865
Hi,
i'm using the adc ADS7865 interfaced with the XINTF peripheral at TMS320C28346.
I checked with the oscilloscope the handshaking line and the timing is corret. In particular I have verify the CONVST signal (I'm using GPIO 56 for this signal) BUSY line and RD, WR and CS lines (these last signals are directly controlled from the XINTF peripheral. I have set single channel and individual CONVST and BUSY for each conversion without sequence. But I'm not able to read the adc result. In particular i have random numbers. The data line is correct because I can set up precisely the DAC out. I'm using the ZONE 0 with the 0x4000 address.
Some one who help me!!!
Thanks.