This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TLV5627: Status of DAC outputs when PD is enabled.

Part Number: TLV5627

What are the state of the output pins when /PD is low? Also, what are the state of the output pins when /PD is high?

  • Hi Sherry,

    Welcome to E2E and thank you for your query. According to the datasheet, making the /PD pin low disables the amplifiers and hence, the output will be 0V or the offset voltage. Making the /PD pin high will enable the amplifiers and hence the output will change according to the code written afterward.

    Regards,
    Uttam Sahu
    Applications Engineer, Precision DACs