Part Number: ADC12DJ3200
1. Was there any application circuit for TMSTP+/-? It say only followings in the datasheet:
TMSTP+/– does not have internal biasing which requires TMSTP+/– to be biased externally whether AC coupled with
TMSTP_LVPECL_EN = 0 or DC coupled with TMSTP_LVPECL_EN = 1
2. It seems supporting LVPECL. Was it LVPECL 2.5V or 3.3V?
3. In the ADC12DJ3200 EVM and TSW14J57EVM or TSW14J56EVM, the differential signals are from FPGA directly. Was it good like this?
Thank you.