Hi,
I'am using dm6467 and tvp5158.
I want to connect 8 analog video inputs coming to DM6467 at D1 resolution, such that each video port on DM6467 can get 4 D1 channels.
I opened PORTA and PORTB, but the data couldn't be captured from the two ports.
The registers of PORTA and PORTB were initialized as the same:
addr value
0x0 0x10
0x1 0xa8
0x2 0x83
0x4 0x2
0x8 0x51
0x9 0x58
0xc 0x81
0xd 0x0
0xe 0xf
0xf 0x3
0x10 0x80
0x11 0x80
0x12 0x0
0x13 0x80
0x14 0x0
0x16 0x10
0x18 0x40
0x19 0x0
0x1a 0x0
0x1b 0x0
0x1c 0xc
0x20 0x0
0x21 0x0
0x23 0x80
0x24 0x0
0x25 0xf5
0x26 0x0
0x27 0x0
0x29 0x6
0x2a 0x1e
0x2b 0x4
0x2c 0x0
0x2d 0xf2
0x2e 0x8
0x34 0x6a
0x35 0x8
0x48 0x7a
0x49 0x0
0x4a 0xd0
0x4b 0x2
0x5c 0x28
0x5d 0x9
0x5e 0x30
0x5f 0x3
0x60 0x0
0x61 0x9
0x7c 0x2
0x7d 0x8
0x7e 0x3
0x7f 0x3
0x80 0xa
0x81 0x0
0x85 0x3
0x86 0x22
0x87 0x0
0x88 0x0
0x89 0x16
0x8c 0x0
0x90 0x10
0x91 0x80
0x92 0x80
0x93 0x0
0x94 0x0
0x95 0x0
0x96 0x60
0x97 0x50
0x9e 0xa
0x9f 0xbc
0xa0 0xbc
0xa2 0xd
0xa3 0x2
0xa8 0x44
0xa9 0x40
0xad 0x0
0xae 0x0
0xaf 0x0
0xb0 0xa0
0xb1 0x11
0xb2 0x2d
0xb3 0xe4
0xb4 0xe4
0xb5 0x0
0xb6 0x1b
0xb7 0x4
0xb8 0x40
0xb9 0x0
0xba 0x0
0xbb 0x1
0xbc 0xd7
0xbd 0xf
0xbe 0x0
0xbf 0x0
0xc0 0x0
0xc1 0x88
0xc2 0x88
0xc3 0xc9
0xc4 0x1
0xc5 0x0
0xc6 0x0
0xc7 0x0
0xc8 0x0
0xc9 0xa5
0xca 0xff
0xcb 0x7e
0xcc 0x1
0xf2 0x0
0xf4 0x0
0xf6 0x0
0xf7 0x0
0xf8 0x0
0xf9 0x25
0xfa 0x25
0xfb 0x25
0xfc 0x25
0xfd 0x25
0xfe 0xf
0xff 0x1
best regards
Armstrong