Other Parts Discussed in Thread: USB2ANY
Hi.
I cannot seem to be able to get the pga900 evm GUI to communicate with the pga900 chip.
It was working fine previously but it somehow just stopped working & I bought a new pga900 chip & still I cannot load firmware on the chip which is frustrating.
Previously when it was working, when the micro is in reset I could read alternating rows of 0x55 and 0xAA in the EEPROM.
I am now not sure if the Evaluation module or usb2any or the GUI is not working. I have downloaded the GUI on another PC and it is the same result.
Is there any way I can check if the usb2any is faulty or if the EVM is faulty? How can I tell which is faulty?
My jumper configuration is 0-10V voltage mode (default configuration except J12 is open & J13 is closed)