Part Number: ADS42LB69
Hello Team,
For ADS42LB69's SYNCIN working theory, I can just found a picture of figure-72 at datasheet, but no more detail description about its whole working process, so some items want to double check with you that:
1. Per figure-72, is it means under SYNC mode, the ADS42LB69 will start the sampling at the 1st rise edge of the CLKIN after the 1st rise edge of SYNCIN? or it's just be my mis-understanding and actually it works at other way?
2. If it start sampling at 1st CLKIN rise edge like above, then a confuse that:
In case there are multi ADS42LB69 on one board, and customer hope to start all device's sampling at the same time per one SYNCIN signal, but each ADS42LB69's CLKIN isn't fully synchronous(a little different time delay), then method above may still cause each ADS42LB69's sampling also have a little different time delay right?
3. For SYNCIN, except sync the sampling, whether it will also sync the output(DBxx, CLKOUT), and if yes how about the sequence between SYNCIN/DBXX/CLKOUT?