Other Parts Discussed in Thread: ADS7841,
Hi
We want to increase precision of AD conversion.
1.
Now we are referring Figure 1.
Is this the best configuration?
For example, would it be better that suppling Vcc and reference voltage sepalately?
Do you have recommended schematic or layout guideline?
2.
I want to confirm reference and COM.
Assumed single-end input,
if reference and VCC are 5V and COM is ground, analog input range would be 0V to 5V.
If reference is 3V, VCC is 5V and COM is 0.5V, analog input range is 0.5V to 3.5V.
Is my understanding correct?
BestRegards