Part Number: ADS7951
Dear all,
I've seen other treads on this topic, but an important spec in the DS is still missing. Which is the ABS MAX value of the REFP pin ?
One of my customer is supplyng the device at 3.3V and it is providing the REFP pin with the same voltage.
The customer does not care too much if there is a degradation of the measurements in this condition, but he needs to know if the part can be damaged.
Usually the Recommended Operating Conditions (max 3V) offer stil some margin. It is the case ? Will the part be damaged if the REFP =3.3V ?
regards,
Domenico