Part Number: ADS1675
Hi, I'm designing a product using TI's ADS1675 and note in the datasheet that the conversion clock for this IC needs to have amplitude equal to AVdd, which is typically 5V (and will be 5V in this design). Since this is a precision application we need a super-low jitter clock, and when I research those parts, all the parts are available in 3.3Vdd or less. Most clock sources with 5V output are legacy devices with unacceptably poor jitter.
What does TI recommend for a super-low jitter 5V clock source? I would be happy to use a logic level translator as long as I can find one with super low injected jitter... although many level translators are not specified for this quantity, so it's not easy finding one. Are there any solid recommendations?
Thanks for reading,
Graham